Data structure of the device_provisioned event.
Public Attribute Documentation#
address#
uint16_t sl_btmesh_evt_prov_device_provisioned_s::address
Address assigned to the node's primary element. If the node has multiple elements, they have been assigned an address in a consecutive sequence following the primary element address.
Definition at line
2377
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uuid#
uuid_128 sl_btmesh_evt_prov_device_provisioned_s::uuid
UUID of the device
Definition at line
2381
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h