Data structure of the initialized event.

Public Attributes#

uint8_t
uint16_t
uint32_t

Public Attribute Documentation#

networks#

uint8_t sl_btmesh_evt_prov_initialized_s::networks

Number of network keys that the Provisioner has


Definition at line 2269 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

address#

uint16_t sl_btmesh_evt_prov_initialized_s::address

Unicast address of the primary element of the Provisioner


Definition at line 2270 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

iv_index#

uint32_t sl_btmesh_evt_prov_initialized_s::iv_index

IVI for network primary network (index 0)


Definition at line 2272 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h