Data structure of the key_refresh_node_update event.

Public Attributes#

uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

key#

uint16_t sl_btmesh_evt_prov_key_refresh_node_update_s::key

Network key index


Definition at line 2608 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

phase#

uint8_t sl_btmesh_evt_prov_key_refresh_node_update_s::phase

Phase moved into


Definition at line 2609 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uuid#

uuid_128 sl_btmesh_evt_prov_key_refresh_node_update_s::uuid

16-byte UUID of the node.


Definition at line 2610 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

failure#

uint8_t sl_btmesh_evt_prov_key_refresh_node_update_s::failure

Shows if the node failed the key refresh phase


Definition at line 2611 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h