Data structure of the oob_auth_request event.
Public Attribute Documentation#
output#
uint8_t sl_btmesh_evt_prov_oob_auth_request_s::output
Zero for static data, non-zero for output
Definition at line
2464
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
output_action#
uint8_t sl_btmesh_evt_prov_oob_auth_request_s::output_action
Enum sl_btmesh_node_oob_output_action_t. Output action type. Ignored for Static.
Definition at line
2465
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
output_size#
uint8_t sl_btmesh_evt_prov_oob_auth_request_s::output_size
Size of output data. Ignored for Static.
Definition at line
2467
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uuid#
uuid_128 sl_btmesh_evt_prov_oob_auth_request_s::uuid
UUID of the device
Definition at line
2468
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h