Data structure of the unprov_beacon event.

Public Attributes#

uint32_t
uint8_t
int8_t

Public Attribute Documentation#

oob_capabilities#

uint16_t sl_btmesh_evt_prov_unprov_beacon_s::oob_capabilities

OOB capabilities bitfield, which indicates the means by which out-of-band provisioning data may be retrieved. See OOB Capabilities.


Definition at line 2402 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uri_hash#

uint32_t sl_btmesh_evt_prov_unprov_beacon_s::uri_hash

Hash of the out-of-band URI, which is received in sl_btmesh_evt_prov_uri. If the URI bit (bit 1) is not set in the OOB capabilities bitfield, this field is ignored.


Definition at line 2406 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

bearer#

uint8_t sl_btmesh_evt_prov_unprov_beacon_s::bearer

Bearer on which the beacon was seen. Values are as follows:

  • 0: PB-ADV

  • 1: PB-GATT


Definition at line 2410 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

address#

bd_addr sl_btmesh_evt_prov_unprov_beacon_s::address

Address of the device beaconing


Definition at line 2414 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

address_type#

uint8_t sl_btmesh_evt_prov_unprov_beacon_s::address_type

Beaconing device address type. Values:

  • 0: Public address

  • 1: Random address


Definition at line 2415 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uuid#

uuid_128 sl_btmesh_evt_prov_unprov_beacon_s::uuid

16-byte UUID of the beaconing device.


Definition at line 2418 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

rssi#

int8_t sl_btmesh_evt_prov_unprov_beacon_s::rssi

RSSI value of the beacon seen. Units: dBm.


Definition at line 2419 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h