Data structure of the filter_status event.

Public Attributes#

uint32_t
uint8_t
uint16_t

Public Attribute Documentation#

handle#

uint32_t sl_btmesh_evt_proxy_filter_status_s::handle

Proxy handle


Definition at line 3669 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

type#

uint8_t sl_btmesh_evt_proxy_filter_status_s::type

Filter type: 0x00 to allow traffic from the given address, 0x01 to block traffic from the given address


Definition at line 3670 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

count#

uint16_t sl_btmesh_evt_proxy_filter_status_s::count

Current filter list length


Definition at line 3672 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h