Data structure of the scan_report event.

Public Attributes#

uint16_t
int8_t
uint16_t
uint32_t

Public Attribute Documentation#

server#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::server

Server address.


Definition at line 19299 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

rssi#

int8_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::rssi

measured signal stength in dBm.


Definition at line 19300 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uuid#

uuid_128 sl_btmesh_evt_remote_provisioning_client_scan_report_s::uuid

UUID of the unprovisioned device found


Definition at line 19301 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

oob#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::oob

OOB information.


Definition at line 19302 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uri#

uint32_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::uri

Hash of the out-of-band URI, which is received in a separate event . If the URI bit (bit 1) is not set in the OOB capabilities bitfield, this field is ignored.


Definition at line 19303 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h