Data structure of the link_open_request event.

Public Attributes#

Public Attribute Documentation#

address#

bd_addr sl_btmesh_evt_remote_provisioning_server_link_open_request_s::address

Address of the device to connect to


Definition at line 19729 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

address_type#

uint8_t sl_btmesh_evt_remote_provisioning_server_link_open_request_s::address_type

Provisinee device address type. Values:

  • 0: Public address

  • 1: Random address


Definition at line 19730 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h