Data structure of the recall event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_scene_server_recall_s::destination_address

Address of the server or the group address to which it was published.


Definition at line 14830 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_scene_server_recall_s::elem_index

Index of the element which received the command.


Definition at line 14832 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

selected_scene#

uint16_t sl_btmesh_evt_scene_server_recall_s::selected_scene

Scene of interest


Definition at line 14834 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_scene_server_recall_s::client_address

Device which sent the request.


Definition at line 14835 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_scene_server_recall_s::appkey_index

Appkey used by client_address.


Definition at line 14836 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transition_time_ms#

uint32_t sl_btmesh_evt_scene_server_recall_s::transition_time_ms

Time (in milliseconds) allotted for the transition to take place


Definition at line 14837 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h