Data structure of the store event.

Public Attributes#

uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::destination_address

Address of the server or the group address to which it was published.


Definition at line 14988 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::elem_index

Index of the element which received the command.


Definition at line 14990 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

scene_id#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::scene_id

Scene ID


Definition at line 14992 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::client_address

Device which sent the request.


Definition at line 14993 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::appkey_index

Appkey used by client_address.


Definition at line 14994 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h