Data structure of the action_status event.
Public Attributes#
uint16_t
uint16_t
uint16_t
uint16_t
uint8_t
uint8_t
uint16_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint32_t
uint16_t
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::client_address
Destination client model address
Definition at line
15139
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::elem_index
Client model element index
Definition at line
15140
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::server_address
Source server model address
Definition at line
15141
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::appkey_index
The application key index to use.
Definition at line
15142
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
index#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::index
Index of the Scheduler Register
Definition at line
15143
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
year#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::year
Scheduled year for the action
Definition at line
15144
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
month#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::month
Scheduled month for the action
Definition at line
15145
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
day#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::day
Scheduled day of the month for the action
Definition at line
15146
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
hour#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::hour
Scheduled hour for the action
Definition at line
15147
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
minute#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::minute
Scheduled minute for the action
Definition at line
15148
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
second#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::second
Scheduled second for the action
Definition at line
15149
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
day_of_week#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::day_of_week
Scheduled days of the week for the action
Definition at line
15150
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
action#
uint8_t sl_btmesh_evt_scheduler_client_action_status_s::action
Action to be performed at the scheduled time
Definition at line
15151
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transition_time_ms#
uint32_t sl_btmesh_evt_scheduler_client_action_status_s::transition_time_ms
Transition time for this action
Definition at line
15152
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
scene_number#
uint16_t sl_btmesh_evt_scheduler_client_action_status_s::scene_number
Scene number to be used for some actions
Definition at line
15153
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h