Data structure of the status event.

Public Attributes#

uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_scheduler_client_status_s::client_address

Destination client model address


Definition at line 15108 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_scheduler_client_status_s::elem_index

Client model element index


Definition at line 15109 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_scheduler_client_status_s::server_address

Source server model address


Definition at line 15110 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_scheduler_client_status_s::appkey_index

The application key index to use.


Definition at line 15111 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

scheduler#

uint16_t sl_btmesh_evt_scheduler_client_status_s::scheduler

Bit field indicating defined Actions in the Schedule Register


Definition at line 15112 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h