Data structure of the action_triggered event.

Public Attributes#

uint16_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_scheduler_server_action_triggered_s::elem_index

Scheduler server model element index


Definition at line 15485 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

index#

uint8_t sl_btmesh_evt_scheduler_server_action_triggered_s::index

Index of the Scheduler Register


Definition at line 15486 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

action#

uint8_t sl_btmesh_evt_scheduler_server_action_triggered_s::action

Action to be performed at the scheduled time


Definition at line 15487 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transition_time_ms#

uint32_t sl_btmesh_evt_scheduler_server_action_triggered_s::transition_time_ms

Transition time for this action


Definition at line 15488 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

scene_number#

uint16_t sl_btmesh_evt_scheduler_server_action_triggered_s::scene_number

Scene number to be used for some actions


Definition at line 15489 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h