Data structure of the model_option_changed event.

Public Attributes#

uint8_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint8_t sl_btmesh_evt_silabs_config_server_model_option_changed_s::elem_index

Element index of model to configure.


Definition at line 22249 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

vendor_id#

uint16_t sl_btmesh_evt_silabs_config_server_model_option_changed_s::vendor_id

Vendor ID of model to configure.


Definition at line 22250 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

model_id#

uint16_t sl_btmesh_evt_silabs_config_server_model_option_changed_s::model_id

Model ID of model to configure.


Definition at line 22251 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

value#

uint16_t sl_btmesh_evt_silabs_config_server_model_option_changed_s::value

Extended packet size to set, currently 1 to use extended 0 to not


Definition at line 22252 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h