Data structure of the network_pdu_changed event.

Public Attributes#

uint16_t

Public Attribute Documentation#

max_size#

uint16_t sl_btmesh_evt_silabs_config_server_network_pdu_changed_s::max_size

Max size of packet to be used, in range 29 - 227 bytes.


Definition at line 22274 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h