Data structure of the replay_protection_list_entry_set event.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

address#

uint16_t sl_btmesh_evt_test_replay_protection_list_entry_set_s::address

Source address for the replay protection list entry


Definition at line 6390 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

cancel#

uint8_t sl_btmesh_evt_test_replay_protection_list_entry_set_s::cancel

Nonzero when replay protection list update relates to a cancelled segmented reception


Definition at line 6391 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h