sl_btmesh_evt_vendor_model_send_complete#

Vendor model message send complete event.

Stack generates this event when a vendor message has been sent or published, either successfully or unsuccessfully.

The time this event is generated depends on the message being sent or published. For an unsegmented message the event is generated immediately after the network PDU is sent out, while for a segmented message the event is generated once the segmented message transmission state machine completes.

Modules#

sl_btmesh_evt_vendor_model_send_complete_s

Macros#

#define
sl_btmesh_evt_vendor_model_send_complete_id 0x011900a8

Identifier of the send_complete event.

Typedef Documentation#

sl_btmesh_evt_vendor_model_send_complete_t#

typedef struct sl_btmesh_evt_vendor_model_send_complete_s sl_btmesh_evt_vendor_model_send_complete_t

Definition at line 4265 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h