Data structure of the default_ttl_status event.

Public Attributes#

uint16_t
uint32_t
uint8_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_config_client_default_ttl_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


handle#

uint32_t sl_btmesh_evt_config_client_default_ttl_status_s::handle

Request handle


value#

uint8_t sl_btmesh_evt_config_client_default_ttl_status_s::value

Default TTL value. Valid value range is from 2 to 127 for relayed PDUs, and 0 to indicate non-relayed PDUs.