Data structure of the heartbeat_sub_status event.

Public Attributes#

uint16_t
uint32_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


handle#

uint32_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::handle

Request handle


source_address#

uint16_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::source_address

Source address for heartbeat messages


destination_address#

uint16_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::destination_address

Destination address for heartbeat messages


period_log#

uint8_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::period_log

Heartbeat subscription remaining period logarithm-of-2 value


count_log#

uint8_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::count_log

Received heartbeat message count logarithm-of-2 value


min_hops#

uint8_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::min_hops

Minimum hop value seen in received heartbeat messages


max_hops#

uint8_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::max_hops

Minimum hop value seen in received heartbeat messages