Data structure of the identity_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_identity_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
value#
uint8_t sl_btmesh_evt_config_client_identity_status_s::value
Identity state of the node for the used network index. Valid values are as follows:
0: Node identity advertising is disabled
1: Node identity advertising is enabled
2: Node identity advertising is not supported