Data structure of the heartbeat event.

Public Attributes#

uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

src_addr#

uint16_t sl_btmesh_evt_node_heartbeat_s::src_addr

Source address for the heartbeat message


Definition at line 841 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

dst_addr#

uint16_t sl_btmesh_evt_node_heartbeat_s::dst_addr

Destination address for the heartbeat message


Definition at line 842 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

hops#

uint8_t sl_btmesh_evt_node_heartbeat_s::hops

Hops traveled by the heartbeat message


Definition at line 843 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h