Data structure of the heartbeat_start event.

Public Attributes#

uint16_t
uint16_t
uint32_t

Public Attribute Documentation#

src_addr#

uint16_t sl_btmesh_evt_node_heartbeat_start_s::src_addr

Source address for the heartbeat message


Definition at line 864 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

dst_addr#

uint16_t sl_btmesh_evt_node_heartbeat_start_s::dst_addr

Destination address for the heartbeat message


Definition at line 865 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

period_sec#

uint32_t sl_btmesh_evt_node_heartbeat_start_s::period_sec

Heartbeat subscription period in seconds.


Definition at line 866 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h