Data structure of the key_added event.

Public Attributes#

uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

type#

uint8_t sl_btmesh_evt_node_key_added_s::type

Type of the new key. Values are as follows:

  • 0x00: Network key

  • 0x01: Application key


Definition at line 647 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

index#

uint16_t sl_btmesh_evt_node_key_added_s::index

Key index of the new key


Definition at line 650 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

netkey_index#

uint16_t sl_btmesh_evt_node_key_added_s::netkey_index

Network key index to which the application key is bound, which is ignored for network keys


Definition at line 651 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h