Data structure of the provisioned event.

Public Attributes#

uint16_t
uint32_t

Public Attribute Documentation#

address#

uint16_t sl_btmesh_evt_node_provisioned_s::address

The unicast address that the Provisioner allocated for the primary element of the node. Secondary elements have been assigned sequentially following unicast addresses.


Definition at line 462 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

iv_index#

uint32_t sl_btmesh_evt_node_provisioned_s::iv_index

Current IV index of the provisioned network


Definition at line 466 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h