Data structure of the capabilities event.

Public Attribute Documentation#

uuid#

uuid_128 sl_btmesh_evt_prov_capabilities_s::uuid

UUID of the device being provisioned


Definition at line 2317 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elements#

uint8_t sl_btmesh_evt_prov_capabilities_s::elements

Number of elements supported by the device


Definition at line 2318 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

algorithms#

uint16_t sl_btmesh_evt_prov_capabilities_s::algorithms

Supported algorithms and other capabilities.


Definition at line 2319 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

pkey_type#

uint8_t sl_btmesh_evt_prov_capabilities_s::pkey_type

Supported public key types


Definition at line 2320 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

static_oob_type#

uint8_t sl_btmesh_evt_prov_capabilities_s::static_oob_type

Supported static OOB Types


Definition at line 2321 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

ouput_oob_size#

uint8_t sl_btmesh_evt_prov_capabilities_s::ouput_oob_size

Maximum size of Output OOB supported


Definition at line 2322 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

output_oob_action#

uint16_t sl_btmesh_evt_prov_capabilities_s::output_oob_action

Supported Output OOB Actions


Definition at line 2323 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

input_oob_size#

uint8_t sl_btmesh_evt_prov_capabilities_s::input_oob_size

Maximum size of input OOB supported


Definition at line 2324 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

intput_oob_action#

uint16_t sl_btmesh_evt_prov_capabilities_s::intput_oob_action

Supported input OOB Actions


Definition at line 2325 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h