Data structure of the ddb_list event.
Public Attribute Documentation#
uuid#
uuid_128 sl_btmesh_evt_prov_ddb_list_s::uuid
UUID of the Device
Definition at line
2529
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
address#
uint16_t sl_btmesh_evt_prov_ddb_list_s::address
Unicast address of the primary element of the node
Definition at line
2530
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elements#
uint8_t sl_btmesh_evt_prov_ddb_list_s::elements
Number of elements the device has
Definition at line
2531
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h