Data structure of the initialized event.
Public Attribute Documentation#
networks#
uint8_t sl_btmesh_evt_prov_initialized_s::networks
Number of network keys that the Provisioner has
Definition at line
2269
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
address#
uint16_t sl_btmesh_evt_prov_initialized_s::address
Unicast address of the primary element of the Provisioner
Definition at line
2270
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
iv_index#
uint32_t sl_btmesh_evt_prov_initialized_s::iv_index
IVI for network primary network (index 0)
Definition at line
2272
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h