Data structure of the provisioning_records_list event.

Public Attributes#

uint16_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_prov_provisioning_records_list_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 2727 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uuid#

uuid_128 sl_btmesh_evt_prov_provisioning_records_list_s::uuid

UUID of the device


Definition at line 2728 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

list#

uint8array sl_btmesh_evt_prov_provisioning_records_list_s::list

Array of 16-bit provisioning record IDs


Definition at line 2729 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h