Data structure of the start_sent event.
Public Attribute Documentation#
uuid#
uuid_128 sl_btmesh_evt_prov_start_sent_s::uuid
UUID of the device
Definition at line
2716
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
algorithm#
uint8_t sl_btmesh_evt_prov_start_sent_s::algorithm
Selected provisioning algorithm
Definition at line
2717
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
public_key#
uint8_t sl_btmesh_evt_prov_start_sent_s::public_key
Selected OOB public key
Definition at line
2718
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
authentication_method#
uint8_t sl_btmesh_evt_prov_start_sent_s::authentication_method
Selected authentication method
Definition at line
2719
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
authentication_action#
uint8_t sl_btmesh_evt_prov_start_sent_s::authentication_action
Selected authentication action
Definition at line
2720
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
authentication_size#
uint8_t sl_btmesh_evt_prov_start_sent_s::authentication_size
Selected authentication size
Definition at line
2721
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h