Data structure of the uri event.
Public Attribute Documentation#
hash#
uint32_t sl_btmesh_evt_prov_uri_s::hash
URI hash. If a Provisioner is provisioning a device which supports out-of-band provisioning and has supplied a URI hash value in its Unprovisioned Device beacon, the Provisioner should check whether the hash matches this value.
Definition at line
2552
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
data#
uint8array sl_btmesh_evt_prov_uri_s::data
Raw URI data, formatted as specified in Bluetooth Core System Supplement v6.
Definition at line
2557
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h