Event Scheduling
Scheduling events for future execution. More...
Macros | |
#define | __EVENT_H__ |
#define | emberEventControlSetInactive(control) do { (control).status = EMBER_EVENT_INACTIVE; } while (0) |
Set this EmberEventControl as inactive (no pending event). More... | |
#define | emberEventControlGetActive(control) ((control).status != EMBER_EVENT_INACTIVE) |
Check whether this EmberEventControl is currently active. An event is considered active if it is set to run some time in the future (activated by emberEventControlSetActive(), emberEventControlSetDelayMS() or any other emberEventControlSetDelay* functions) More... | |
#define | emberEventControlSetActive(control) do { emEventControlSetActive(&(control)); } while (0) |
Set this EmberEventControl to run at the next available opportunity. More... | |
#define | EMBER_MAX_EVENT_CONTROL_DELAY_MS (HALF_MAX_INT32U_VALUE - 1) |
The maximum delay that may be passed to emberEventControlSetDelayMS(). More... | |
#define | emberEventControlSetDelayMS(control, delay) do { emEventControlSetDelayMS(&(control), (delay)); } while (0) |
Set this EmberEventControl to run some milliseconds in the future. More... | |
#define | EMBER_MAX_EVENT_CONTROL_DELAY_QS (EMBER_MAX_EVENT_CONTROL_DELAY_MS >> 8) |
The maximum delay that may be passed to emberEventControlSetDelayQS(). More... | |
#define | emberEventControlSetDelayQS(control, delay) do { emEventControlSetDelayMS(&(control), (delay) << 8); } while (0) |
Set this EmberEventControl to run some quarter seconds in the future. More... | |
#define | EMBER_MAX_EVENT_CONTROL_DELAY_MINUTES (EMBER_MAX_EVENT_CONTROL_DELAY_MS >> 16) |
The maximum delay that may be passed to emberEventControlSetDelayMinutes(). More... | |
#define | emberEventControlSetDelayMinutes(control, delay) do { emEventControlSetDelayMS(&(control), (delay) << 16); } while (0) |
Set this EmberEventControl to run some minutes in the future. More... | |
#define | emberEventControlGetRemainingMS(control) (emEventControlGetRemainingMS(&(control))) |
Check when the event is scheduled to run. More... | |
#define | emberTaskEnableIdling(allow) do { emTaskEnableIdling((allow)); } while (0) |
Enable or disable idling. More... | |
#define | emberMarkTaskActive(taskid) do { emMarkTaskActive((taskid)); } while (0) |
Calling it indicates that a task has something to do, so it should prevent the CPU from idling until emberMarkTaskIdle is next called on this task. More... | |
Functions | |
void | emEventControlSetActive (EmberEventControl *event) |
void | emEventControlSetDelayMS (EmberEventControl *event, uint32_t delay) |
uint32_t | emEventControlGetRemainingMS (EmberEventControl *event) |
void | emberRunEvents (EmberEventData *events) |
Start an event handler if there is anything scheduled at the moment this function is called. More... | |
void | emberRunTask (EmberTaskId taskid) |
Start an event handler if there is anything scheduled at the moment this function is called. More... | |
uint32_t | emberMsToNextEvent (EmberEventData *events, uint32_t maxMs) |
Check when the next event is scheduled to run. More... | |
uint32_t | emberMsToNextEventExtended (EmberEventData *events, uint32_t maxMs, uint8_t *returnIndex) |
uint32_t | emberMsToNextStackEvent (void) |
Check when the next stack event is scheduled to run. More... | |
EmberTaskId | emberTaskInit (EmberEventData *events) |
Initialize a task for managing events and processor idling state. More... | |
bool | emberMarkTaskIdle (EmberTaskId taskid) |
Try to idle the CPU, unless any events in any tasks are pending. More... | |
void | emTaskEnableIdling (bool allow) |
Enable or disable idling. More... | |
void | emMarkTaskActive (EmberTaskId taskid) |
Calling it indicates that a task has something to do, so it should prevent the CPU from idling until emberMarkTaskIdle is next called on this task. More... | |
Detailed Description
Scheduling events for future execution.
See Event Scheduling for documentation. These macros implement an event abstraction that allows the application to schedule code to run after a specified time interval. An event consists of a procedure to be called at some point in the future and a control object that determines which procedure should be called. Events are also useful when an ISR needs to initiate an action that should run outside the ISR context.
See event.h
for source code.
Note that, while not required, it is recommended that the event-handling procedure explicitly define the recurrence of the next event, either by rescheduling via some kind of emberEventControlSetDelayXX() call or by deactivating via a call to emberEventControlSetInactive().
When the handler does not explicitly reschedule or cancel the event, the default behavior of the event control system is to keep the event immediately active as if the handler function had called emberEventControlSetActive(someEvent) or emberEventControlSetDelayMS(someEvent, 0).
The base time units for events are ticks. A tick equals 1us on every platform supported by Connect. Note, however, that the accuracy of the base tick depends on the timer source, which by default is the LF RC oscillator on EFR32 platforms.
Furthermore, the scheduled delay is the minimum delay. If emberRunEvents() or emberRunTask() are not called frequently enough, the actual delay may be longer than the scheduled delay.
Additionally, the APIs for quarter second and minute delays (emberEventControlSetDelayQS() and emberEventControlSetDelayMinutes()) use "binary" units. One quarter second is 256 ticks and one minute is 65536 ticks. These APIs are therefore doesn't actually mean a quarter of second or a minute on platforms supported by Connect.
However, in the future, Connect support might become available on platforms where one tick is not exactly 1us. For example,. on the EM357 SoC, 1ms is 1024 ticks, so each tick is 1000 / 1024 = ~0.98 milliseconds. If you need platform independent accurate delays, use the macros ::MILLISECOND_TICKS_PER_SECOND and ::MILLISECOND_TICKS_PER_MINUTE. For example, calling emberEventControlSetDelayMS(someEvent, 3 * MILLISECOND_TICKS_PER_MINUTE) will delay for 3 minutes on any platform.
The following are brief usage examples.
Macro Definition Documentation
◆ __EVENT_H__
#define __EVENT_H__ |
Definition at line 166
of file event.h
.
◆ EMBER_MAX_EVENT_CONTROL_DELAY_MINUTES
#define EMBER_MAX_EVENT_CONTROL_DELAY_MINUTES (EMBER_MAX_EVENT_CONTROL_DELAY_MS >> 16) |
The maximum delay that may be passed to emberEventControlSetDelayMinutes().
Definition at line 252
of file event.h
.
◆ EMBER_MAX_EVENT_CONTROL_DELAY_MS
#define EMBER_MAX_EVENT_CONTROL_DELAY_MS (HALF_MAX_INT32U_VALUE - 1) |
The maximum delay that may be passed to emberEventControlSetDelayMS().
Definition at line 210
of file event.h
.
◆ EMBER_MAX_EVENT_CONTROL_DELAY_QS
#define EMBER_MAX_EVENT_CONTROL_DELAY_QS (EMBER_MAX_EVENT_CONTROL_DELAY_MS >> 8) |
The maximum delay that may be passed to emberEventControlSetDelayQS().
Definition at line 235
of file event.h
.
◆ emberEventControlGetActive
#define emberEventControlGetActive | ( | control | ) | ((control).status != EMBER_EVENT_INACTIVE) |
Check whether this EmberEventControl is currently active. An event is considered active if it is set to run some time in the future (activated by emberEventControlSetActive(), emberEventControlSetDelayMS() or any other emberEventControlSetDelay* functions)
- Parameters
-
[in] control
Control of the event in question.
- Returns
- Returns true if the event is active false otherwise
Definition at line 187
of file event.h
.
◆ emberEventControlGetRemainingMS
#define emberEventControlGetRemainingMS | ( | control | ) | (emEventControlGetRemainingMS(&(control))) |
Check when the event is scheduled to run.
- Parameters
-
[in] control
Control of the event in question.
- Returns
- Returns the amount of milliseconds remaining before the event is scheduled to run. If the event is inactive, MAX_INT32U_VALUE is returned.
Definition at line 271
of file event.h
.
◆ emberEventControlSetActive
#define emberEventControlSetActive | ( | control | ) | do { emEventControlSetActive(&(control)); } while (0) |
Set this EmberEventControl to run at the next available opportunity.
- Parameters
-
[in] control
Control of the event to set active.
Definition at line 196
of file event.h
.
◆ emberEventControlSetDelayMinutes
#define emberEventControlSetDelayMinutes | ( | control, |
|
delay |
|||
) | do { emEventControlSetDelayMS(&(control), (delay) << 16); } while (0) |
Set this EmberEventControl to run some minutes in the future.
- Parameters
-
[in] control
Control of the event to run. [in] delay
The delay in minute. One minute is actually 65536 ms. Must be less than EMBER_MAX_EVENT_CONTROL_DELAY_MINUTES
Definition at line 261
of file event.h
.
◆ emberEventControlSetDelayMS
#define emberEventControlSetDelayMS | ( | control, |
|
delay |
|||
) | do { emEventControlSetDelayMS(&(control), (delay)); } while (0) |
Set this EmberEventControl to run some milliseconds in the future.
- Parameters
-
[in] control
Control of the event to run. [in] delay
The delay in milliseconds. Must be less than EMBER_MAX_EVENT_CONTROL_DELAY_MS
Definition at line 219
of file event.h
.
◆ emberEventControlSetDelayQS
#define emberEventControlSetDelayQS | ( | control, |
|
delay |
|||
) | do { emEventControlSetDelayMS(&(control), (delay) << 8); } while (0) |
Set this EmberEventControl to run some quarter seconds in the future.
- Parameters
-
[in] control
Control of the event to run. [in] delay
The delay in quarter seconds. One quarter second is actually 256 ms. Must be less than EMBER_MAX_EVENT_CONTROL_DELAY_QS
- Warning
- Applications should use emberEventControlSetDelayQS() instead.
Definition at line 246
of file event.h
.
◆ emberEventControlSetInactive
#define emberEventControlSetInactive | ( | control | ) | do { (control).status = EMBER_EVENT_INACTIVE; } while (0) |
Set this EmberEventControl as inactive (no pending event).
- Parameters
-
[in] control
Control of the event to set inactive.
Definition at line 173
of file event.h
.
◆ emberMarkTaskActive
#define emberMarkTaskActive | ( | taskid | ) | do { emMarkTaskActive((taskid)); } while (0) |
Calling it indicates that a task has something to do, so it should prevent the CPU from idling until emberMarkTaskIdle is next called on this task.
- Parameters
-
[in] taskid
The task to mark active.
Definition at line 397
of file event.h
.
◆ emberTaskEnableIdling
#define emberTaskEnableIdling | ( | allow | ) | do { emTaskEnableIdling((allow)); } while (0) |
Enable or disable idling.
- Parameters
-
[in] allow
Setting it to true will enable, while setting it to false will disable idling.
Definition at line 382
of file event.h
.
Function Documentation
◆ emberMarkTaskIdle()
bool emberMarkTaskIdle | ( | EmberTaskId | taskid | ) |
Try to idle the CPU, unless any events in any tasks are pending.
- Parameters
-
[in] taskid
the task which should handle the idling.
- Returns
- Returns true if the processor was idled false if idling wasn't permitted because a task has something to do.
- Note
- This API should always be called with interrupts disabled. It will forcibly re-enable interrupts before returning.
◆ emberMsToNextEvent()
uint32_t emberMsToNextEvent | ( | EmberEventData * | events, |
uint32_t | maxMs |
||
) |
Check when the next event is scheduled to run.
- Parameters
-
[in] events
An array of events to check. [in] maxMs
If no event is scheduled before maxMs, maxMs will be returned
- Returns
- Returns the number of milliseconds before the next event is scheduled to expire, or
maxMs
if no event is scheduled to expire within that time.
- Note
- If any events are modified within an interrupt, to guarantee the accuracy of this API, it must be called with interrupts disabled.
- See also
- emberMsToNextEventExtended()
◆ emberMsToNextEventExtended()
uint32_t emberMsToNextEventExtended | ( | EmberEventData * | events, |
uint32_t | maxMs, |
||
uint8_t * | returnIndex |
||
) |
Check when the next event is scheduled to run.
- Parameters
-
[in] events
An array of events to check. [in] maxMs
If no event is scheduled before maxMs, maxMs will be returned [out] returnIndex
If not NULL pointer was passed, the index of the next event will be returned here, or 0xFF if no event is scheduled before maxMs.
- Returns
- Returns the number of milliseconds before the next event is scheduled to expire, or
maxMs
if no event is scheduled to expire within that time.
- Note
- If any events are modified within an interrupt, to guarantee the accuracy of this API, it must be called with interrupts disabled.
- See also
- emberMsToNextEvent()
◆ emberMsToNextStackEvent()
uint32_t emberMsToNextStackEvent | ( | void |
| ) |
Check when the next stack event is scheduled to run.
- Returns
- Returns the number of milliseconds before the next stack event is scheduled to run.
◆ emberRunEvents()
void emberRunEvents | ( | EmberEventData * | events | ) |
Start an event handler if there is anything scheduled at the moment this function is called.
An application typically creates an array of events along with their handlers. This function should be called in the main loop to run those events.
- Parameters
-
[in] events
Pointer to the array of events.
- Warning
- This is normally handled by emberRunTask() in the main plugin.
◆ emberRunTask()
void emberRunTask | ( | EmberTaskId | taskid | ) |
Start an event handler if there is anything scheduled at the moment this function is called.
If an application has initialized a task via emberTaskInit(), to run the events associated with that task, it should call emberRunTask() instead of emberRunEvents().
- Warning
- This is normally handled by the main plugin.
◆ emberTaskInit()
EmberTaskId emberTaskInit | ( | EmberEventData * | events | ) |
Initialize a task for managing events and processor idling state.
- Parameters
-
[in] events
Pointer to the array of events to manage
- Returns
- Returns the EmberTaskId which represents the newly created task.
- Note
- After the task is created emberRunTask() should be called periodically.
◆ emEventControlGetRemainingMS()
uint32_t emEventControlGetRemainingMS | ( | EmberEventControl * | event | ) |
Check when the event is scheduled to run.
- Parameters
-
[in] event
Pointer to the control of the event in question.
- Returns
- Return the amount of milliseconds remaining before the event is scheduled to run. If the event is inactive, MAX_INT32U_VALUE is returned.
- Warning
- Applications should use emberEventControlGetRemainingMS() instead.
◆ emEventControlSetActive()
void emEventControlSetActive | ( | EmberEventControl * | event | ) |
Set this EmberEventControl to run at the next available opportunity.
- Parameters
-
[in] event
Pointer to the control of the event to set active
- Warning
- Applications should use emberEventControlSetActive() instead.
◆ emEventControlSetDelayMS()
void emEventControlSetDelayMS | ( | EmberEventControl * | event, |
uint32_t | delay |
||
) |
Set this EmberEventControl to run some milliseconds in the future.
- Parameters
-
[in] event
Pointer to the control of the event to run. [in] delay
The delay in milliseconds. Must be less than EMBER_MAX_EVENT_CONTROL_DELAY_MS
- Warning
- Applications should use emberEventControlSetDelayMS() instead.
◆ emMarkTaskActive()
void emMarkTaskActive | ( | EmberTaskId | taskid | ) |
Calling it indicates that a task has something to do, so it should prevent the CPU from idling until emberMarkTaskIdle is next called on this task.
- Parameters
-
[in] taskid
The task to mark active.
- Warning
- Applications should use emberMarkTaskActive() instead.
◆ emTaskEnableIdling()
void emTaskEnableIdling | ( | bool | allow | ) |
Enable or disable idling.
- Parameters
-
[in] allow
Setting it to true will enable, while setting it to false will disable idling.
- Warning
- Applications should use emberTaskEnableIdling() instead.