Stack Counters
Stack counters API. More...
Functions | |
EmberStatus | emberGetCounter (EmberCounterType counterType, uint32_t *count) |
Retrieve the stack counter corresponding to the passed counter type. More... | |
Detailed Description
Stack counters API.
Function Documentation
◆ emberGetCounter()
EmberStatus emberGetCounter | ( | EmberCounterType | counterType, |
uint32_t * | count |
||
) |
Retrieve the stack counter corresponding to the passed counter type.
- Parameters
-
[in] counterType
An EmberCounterType value indicating the stack counter to be retrieved. [out] count
The counter of the requested counterType
is returned here
- Returns
- An EmberStatus value of EMBER_SUCCESS if the stack counter was successfully retrieved. An EmberStatus value of EMBER_INVALID_CALL if the passed counterType is invalid. An EmberStatus value of EMBER_LIBRARY_NOT_PRESENT if the stack counter library is not present.