tokTypeStackChildTableEntry Struct Reference
Type of an element of TOKEN_STACK_CHILD_TABLE (indexed token). Keeps children information of a device, which has parent support enabled. More...
#include <
token-stack.h
>
Data Fields | |
EmberEUI64 | longId |
EmberNodeId | shortId |
uint8_t | flags |
Type of an element of TOKEN_STACK_CHILD_TABLE (indexed token). Keeps children information of a device, which has parent support enabled.
Definition at line 245
of file token-stack.h
.
Field Documentation
◆ flags
uint8_t tokTypeStackChildTableEntry::flags |
Flags for the child required by the stack
Definition at line 248
of file token-stack.h
.
◆ longId
EmberEUI64 tokTypeStackChildTableEntry::longId |
The Long Id of the child
Definition at line 246
of file token-stack.h
.
◆ shortId
EmberNodeId tokTypeStackChildTableEntry::shortId |
The NodeId of the child
Definition at line 247
of file token-stack.h
.
The documentation for this struct was generated from the following file:
token-stack.h