EmberTaskControl Struct Reference

Control structure for tasks. More...

#include < ember-types.h >

Data Fields

uint32_t nextEventTime
EmberEventData * events
bool busy

Control structure for tasks.

This structure should not be accessed directly.

Definition at line 589 of file ember-types.h .

Field Documentation

◆ busy

bool EmberTaskControl::busy

A flag that indicates the task has something to do other than events

Definition at line 595 of file ember-types.h .

◆ events

EmberEventData * EmberTaskControl::events

The list of events associated with this task

Definition at line 593 of file ember-types.h .

◆ nextEventTime

uint32_t EmberTaskControl::nextEventTime

The time when the next event associated with this task will fire

Definition at line 591 of file ember-types.h .


The documentation for this struct was generated from the following file:
  • ember-types.h