Network Management
Connect API for finding, forming, joining, and leaving Connect networks. More...
Modules |
|
| Frequency Hopping | |
|
API and callbacks for frequency hopping configuration.
|
|
| Parent Support | |
Macros |
|
| #define | EMBER_MAC_MAX_APP_BEACON_PAYLOAD_LENGTH 16 |
|
The maximum length in bytes of the application beacon payload.
More...
|
|
| #define | EMBER_MAC_MAX_BEACON_FIELDS_LENGTH 84 |
|
The maximum length in bytes of the beacon fields (superframe, GTS, pending address) as per 802.15.4 specs.
More...
|
|
| #define | EMBER_CHILD_TABLE_AGING_DISABLED 0x20C400 |
|
A special timeout value that disables aging of the child table.
More...
|
|
| #define | EMBER_CHILD_TABLE_MAX_TIMEOUT_S ( EMBER_CHILD_TABLE_AGING_DISABLED - 1) |
|
The maximum timeout in seconds after which a stale entry may be removed from the child table.
More...
|
|
| #define | EMBER_MAX_SELECTIVE_JOIN_PAYLOAD_LENGTH 50 |
|
The maximum length in bytes of the join payload.
More...
|
|
| #define | EMBER_MAX_AUXILIARY_ADDRESS_FILTERING_TABLE_LENGTH 2 |
|
The maximum number of entries the auxiliary address filtering table can hold.
More...
|
|
Functions |
|
| EmberStatus | emberInit (void) |
|
Initialize the radio and the Ember stack.
More...
|
|
| void | emberTick (void) |
|
A periodic tick routine that should be called in the main loop in the application.
More...
|
|
| EmberStatus | emberNetworkInit (void) |
|
Resume the network operation after a reboot.
More...
|
|
| EmberStatus | emberStartActiveScan (uint16_t channel) |
|
Start an active scan.
EMBER_SUCCESS
signals that the scan successfully started. Upon receiving a beacon, the
emberIncomingBeaconHandler()
stack handler is called. At the end of the scanning procedure, the
emberActiveScanCompleteHandler()
stack handler is called. Note that, while a scan can be initiated when the node is currently joined to a network, the node will generally be unable to communicate with its PAN during the scan period. In particular, time-sensitive network operations might be affected because a scan operation will prevent any network operation for the duration of the scan.
More...
|
|
| EmberStatus | emberSetActiveScanDuration (uint16_t durationMs) |
|
Set the time in milliseconds the node will spend listening for incoming beacons during an active scan. The dafault value is set based on the symbol time of the current PHY configuration according to the 802.15.4 specs.
More...
|
|
| uint16_t | emberGetActiveScanDuration (void) |
|
Get the current active scan duration in milliseconds.
More...
|
|
| EmberStatus | emberStartEnergyScan (uint16_t channel, uint8_t samples) |
|
Starts an energy scan.
EMBER_SUCCESS
signals that the scan successfully started. At the end of the scanning procedure the
emberEnergyScanCompleteHandler()
stack handler is called. Note that, while a scan can be initiated when the node is currently joined to a network, the node is generally unable to communicate with its PAN during the scan period. In particular, time-sensitive network operations might be affected because a scan operation will prevent any network operation for the duration of the scan.
More...
|
|
| EmberStatus | emberSetApplicationBeaconPayload (uint8_t payloadLength, uint8_t *payload) |
|
Allows the application to set the application portion of the beacon payload. It's by default set to the empty string.
More...
|
|
| EmberStatus | emberJoinNetworkExtended ( EmberNodeType nodeType, EmberNodeId nodeId, EmberNetworkParameters *parameters) |
|
Cause the stack to associate with the network using the specified network parameters. It can take several seconds for the stack to associate with the local network. Do not send messages until a call to the
emberStackStatusHandler()
callback informs you that the stack is up. Notice that forming a network causes the node's security frame counter to be reset.
More...
|
|
| EmberStatus | emberJoinNetwork ( EmberNodeType nodeType, EmberNetworkParameters *parameters) |
|
Cause the stack to associate with the network using the specified network parameters. The network ID is assigned by the network coordinator. It can take several seconds for the stack to associate with the local network. Do not send messages until a call to the
emberStackStatusHandler()
callback informs you that the stack is up. Notice that joining a network causes the node's security frame counter to be reset.
More...
|
|
| EmberStatus | emberPermitJoining (uint8_t duration) |
|
Tell the stack to allow other nodes to join the network with this node as their parent. Joining is initially disabled by default. This function may only be called after the node is part of a network and the stack is up.
More...
|
|
| EmberStatus | emberJoinCommissioned ( EmberNodeType nodeType, EmberNodeId nodeId, EmberNetworkParameters *parameters) |
|
Cause the stack to go up with the passed network parameters without performing any over-the-air message exchange. Notice that commissioning a network causes the node's security frame counter to be reset.
More...
|
|
| EmberStatus | emberSetSelectiveJoinPayload (uint8_t payloadLength, uint8_t *payload) |
|
When invoked at a
EMBER_STAR_COORDINATOR
or a
EMBER_STAR_RANGE_EXTENDER
, it causes the stack to only accept subsequent joining nodes with matching joining payload. When invoked at a node that has not yet joined a network, it sets the joining payload that will be included in the joining process. Notice, the join payload is included in a non-standard 802.15.4 command, therefore this feature is not available for nodes operating as
EMBER_MAC_MODE_DEVICE
or
EMBER_MAC_MODE_SLEEPY_DEVICE
.
More...
|
|
| EmberStatus | emberClearSelectiveJoinPayload (void) |
|
Clear the join payload previously set with the
emberSetSelectiveJoinPayload()
API. When invoked at an
EMBER_STAR_COORDINATOR
or an
EMBER_STAR_RANGE_EXTENDER
it causes the stack to accept joining nodes with any join payload pattern. When invoked at a node that has not yet joined a network, it clears the join payload. Subsequent joining attempts will not include any join payload in the over-the-air joining handshake.
More...
|
|
| EmberStatus | emberSetAuxiliaryAddressFilteringEntry ( EmberNodeId nodeId, uint8_t entryIndex) |
|
Set an entry in the auxiliary address filtering table at a given address. Nodes of
EMBER_DIRECT_DEVICE
device type can receive incoming messages destined to any of the node IDs in the auxiliary address filtering table (while also receiving messages destined to actual node ID). If the passed node ID is
EMBER_NULL_NODE_ID
, the entry is cleared.
More...
|
|
| EmberNodeId | emberGetAuxiliaryAddressFilteringEntry (uint8_t entryIndex) |
|
Retrieve the content of the auxiliary address filtering table at a given address. See
emberSetAuxiliaryAddressFilteringEntry()
for details.
More...
|
|
| void | emberResetNetworkState (void) |
|
Forget the current network and reverts to a network status of
EMBER_NO_NETWORK
.
More...
|
|
| EmberStatus | emberMacFormNetwork ( EmberNetworkParameters *parameters) |
|
Form a new network as an
EMBER_MAC_MODE_DEVICE
by becoming the coordinator. This API should be used to form a compliant 802.15.4 PAN and to inter-operate with other 802.15.4 devices. Notice that forming a network causes the node's security frame counter to be reset.
More...
|
|
| EmberStatus | emberMacSetPanCoordinator (bool isCoordinator) |
|
Configure a
EMBER_MAC_MODE_DEVICE
node to be a PAN coordinator. Note, this only applies to nodes that have been commissioned as
EMBER_MAC_MODE_DEVICE
.
More...
|
|
| EmberStatus | emberNetworkLeave (void) |
|
Allow a star topology node that previously joined a network to leave the network. The node will notify the parent node and eventually leave the network. The application is notified that the leave procedure completed via the
emberStackStatusHandler()
handler.
More...
|
|
| EmberStatus | emberMacAddShortToLongAddressMapping ( EmberNodeId shortId, EmberEUI64 longId) |
|
An API to populate the short-to-long address mapping table at the MAC layer. The table is meaningful only when running as
EMBER_MAC_MODE_DEVICE
or
EMBER_MAC_MODE_SLEEPY_DEVICE
. The standard 802.15.4 encryption and authentication process requires the security nonce to be populated with the source node long ID. A receiver must do the same to decrypt a secured incoming message. This short-to-long mapping table is used to decrypt a secured incoming packet from a node using short source addressing. If no entry is found in this table, the incoming message will be dropped. This table is also used to encrypt secured outgoing messages with short source addressing in case the node is sending out a secured message with a short source address other than its own.
More...
|
|
| EmberStatus | emberMacClearShortToLongAddressMappings (void) |
|
An API to clear the short-to-long address mapping table at the MAC layer.
More...
|
|
Handlers |
|
| void | emberIncomingBeaconHandler ( EmberPanId panId, EmberMacAddress *source, int8_t rssi, bool permitJoining, uint8_t beaconFieldsLength, uint8_t *beaconFields, uint8_t beaconPayloadLength, uint8_t *beaconPayload) |
|
This stack handler is invoked if a beacon is received during the scanning procedure if this was initiated by the application with the
emberStartActiveScan()
stack APIs.
More...
|
|
| void | emberActiveScanCompleteHandler (void) |
|
This stack handler is invoked after the application calls the
emberStartActiveScan()
stack API to inform the application that the scanning procedure is complete.
More...
|
|
| void | emberEnergyScanCompleteHandler (int8_t mean, int8_t min, int8_t max, uint16_t variance) |
|
This stack handler is invoked after the application calls the
emberStartEnergyScan()
stack API to inform the application that the energy scan procedure is complete and to provide statistics.
More...
|
|
Detailed Description
Connect API for finding, forming, joining, and leaving Connect networks.
See
network-management.h
for source code.
Macro Definition Documentation
◆ EMBER_CHILD_TABLE_AGING_DISABLED
| #define EMBER_CHILD_TABLE_AGING_DISABLED 0x20C400 |
A special timeout value that disables aging of the child table.
Definition at line
40
of file
network-management.h
.
◆ EMBER_CHILD_TABLE_MAX_TIMEOUT_S
| #define EMBER_CHILD_TABLE_MAX_TIMEOUT_S ( EMBER_CHILD_TABLE_AGING_DISABLED - 1) |
The maximum timeout in seconds after which a stale entry may be removed from the child table.
Definition at line
45
of file
network-management.h
.
◆ EMBER_MAC_MAX_APP_BEACON_PAYLOAD_LENGTH
| #define EMBER_MAC_MAX_APP_BEACON_PAYLOAD_LENGTH 16 |
The maximum length in bytes of the application beacon payload.
Definition at line
31
of file
network-management.h
.
◆ EMBER_MAC_MAX_BEACON_FIELDS_LENGTH
| #define EMBER_MAC_MAX_BEACON_FIELDS_LENGTH 84 |
The maximum length in bytes of the beacon fields (superframe, GTS, pending address) as per 802.15.4 specs.
Definition at line
36
of file
network-management.h
.
◆ EMBER_MAX_AUXILIARY_ADDRESS_FILTERING_TABLE_LENGTH
| #define EMBER_MAX_AUXILIARY_ADDRESS_FILTERING_TABLE_LENGTH 2 |
The maximum number of entries the auxiliary address filtering table can hold.
Definition at line
396
of file
network-management.h
.
◆ EMBER_MAX_SELECTIVE_JOIN_PAYLOAD_LENGTH
| #define EMBER_MAX_SELECTIVE_JOIN_PAYLOAD_LENGTH 50 |
The maximum length in bytes of the join payload.
Definition at line
358
of file
network-management.h
.
Function Documentation
◆ emberActiveScanCompleteHandler()
| void emberActiveScanCompleteHandler | ( | void |
|
) |
This stack handler is invoked after the application calls the emberStartActiveScan() stack API to inform the application that the scanning procedure is complete.
◆ emberClearSelectiveJoinPayload()
| EmberStatus emberClearSelectiveJoinPayload | ( | void |
|
) |
Clear the join payload previously set with the emberSetSelectiveJoinPayload() API. When invoked at an EMBER_STAR_COORDINATOR or an EMBER_STAR_RANGE_EXTENDER it causes the stack to accept joining nodes with any join payload pattern. When invoked at a node that has not yet joined a network, it clears the join payload. Subsequent joining attempts will not include any join payload in the over-the-air joining handshake.
- Returns
-
An
EmberStatusvalue that indicates either:- that the node successfully cleared the join payload.
- the reason for failure.
◆ emberEnergyScanCompleteHandler()
| void emberEnergyScanCompleteHandler | ( | int8_t |
mean,
|
| int8_t |
min,
|
||
| int8_t |
max,
|
||
| uint16_t |
variance
|
||
| ) |
This stack handler is invoked after the application calls the emberStartEnergyScan() stack API to inform the application that the energy scan procedure is complete and to provide statistics.
- Parameters
-
[in] meanThe average energy detected in dBm. [in] minThe minimum energy detected in dBm. [in] maxThe maximum energy detected in dBm. [in] varianceThe variance of the energy detected in dBm.
◆ emberGetActiveScanDuration()
| uint16_t emberGetActiveScanDuration | ( | void |
|
) |
Get the current active scan duration in milliseconds.
- Returns
- a 16-bit integer indicating the current duration in millisecond of the active scan.
◆ emberGetAuxiliaryAddressFilteringEntry()
| EmberNodeId emberGetAuxiliaryAddressFilteringEntry | ( | uint8_t |
entryIndex
|
) |
Retrieve the content of the auxiliary address filtering table at a given address. See emberSetAuxiliaryAddressFilteringEntry() for details.
- Parameters
-
[in] entryIndexThe index in the auxiliary address filtering table entry to be retrieved.
- Returns
- An EmberNodeId value of EMBER_NULL_NODE_ID if the passed entry index is invalid or if the passed entry index refers to an unused entry. Otherwise, it returns the content of the auxiliary address filtering table entry corresponding to the passed entry index.
◆ emberIncomingBeaconHandler()
| void emberIncomingBeaconHandler | ( | EmberPanId |
panId,
|
| EmberMacAddress * |
source,
|
||
| int8_t |
rssi,
|
||
| bool |
permitJoining,
|
||
| uint8_t |
beaconFieldsLength,
|
||
| uint8_t * |
beaconFields,
|
||
| uint8_t |
beaconPayloadLength,
|
||
| uint8_t * |
beaconPayload
|
||
| ) |
This stack handler is invoked if a beacon is received during the scanning procedure if this was initiated by the application with the emberStartActiveScan() stack APIs.
- Parameters
-
[in] panIdThe source pan ID of the received beacon. [in] sourceThe source node address of the received beacon. [in] rssiThe RSSI the beacon was received with. [in] permitJoiningThe permit joining flag in the received beacon. [in] beaconFieldsLengthThe length in bytes of the beacon fields defined as per 802.15.4 specs (superframe, GTS fields and pending address fields) of the received beacon. [in] beaconFieldsA pointer to the the beacon fields defined as per 802.15.4 specs (superframe, GTS fields and pending address fields) of the received beacon. [in] beaconPayloadLengthThe length in bytes of the application beacon payload of the received beacon. [in] beaconPayloadA pointer to the application beacon payload of the received beacon.
◆ emberInit()
| EmberStatus emberInit | ( | void |
|
) |
Initialize the radio and the Ember stack.
Device configuration functions must be called before emberInit() is called.
- Note
- The application must check the return value of this function. If the initialization fails, normal messaging functions are not available. Some failure modes are not fatal, but the application must follow certain procedures to permit recovery. Ignoring the return code results in unpredictable radio and API behavior. (In particular, problems with association will occur.)
- Returns
-
An
EmberStatusvalue indicating successful initialization or the reason for failure.
◆ emberJoinCommissioned()
| EmberStatus emberJoinCommissioned | ( | EmberNodeType |
nodeType,
|
| EmberNodeId |
nodeId,
|
||
| EmberNetworkParameters * |
parameters
|
||
| ) |
Cause the stack to go up with the passed network parameters without performing any over-the-air message exchange. Notice that commissioning a network causes the node's security frame counter to be reset.
- Parameters
-
[in] nodeTypeSpecifies the role that this node will have in the network. The only device types allowed in the commissioning API are EMBER_DIRECT_DEVICE , EMBER_MAC_MODE_DEVICE and EMBER_MAC_MODE_SLEEPY_DEVICE . [in] nodeIdAn EmberNodeId value that specifies the short ID the node will have. The passed node ID must be a valid short address (any value other than EMBER_NULL_NODE_ID or EMBER_BROADCAST_ADDRESS ). A value of EMBER_USE_LONG_ADDRESS is allowed only when commissioning the node as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE and will cause the node to send MAC level control messages such as data polls or beacons using long source addressing. [in] parametersAn EmberNetworkParameters value that specifies the network parameters of the network the node should participate in.
- Returns
-
An
EmberStatusvalue that indicates either:- that the node successfully commissioned the passed network parameters
- the reason for failure.
◆ emberJoinNetwork()
| EmberStatus emberJoinNetwork | ( | EmberNodeType |
nodeType,
|
| EmberNetworkParameters * |
parameters
|
||
| ) |
Cause the stack to associate with the network using the specified network parameters. The network ID is assigned by the network coordinator. It can take several seconds for the stack to associate with the local network. Do not send messages until a call to the emberStackStatusHandler() callback informs you that the stack is up. Notice that joining a network causes the node's security frame counter to be reset.
- Parameters
-
[in] nodeTypeSpecification of the role that this node will have in the network. This role can be EMBER_STAR_RANGE_EXTENDER , EMBER_STAR_END_DEVICE , EMBER_STAR_SLEEPY_END_DEVICE , EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE . If the node is frequency hopping, the role can not be EMBER_STAR_RANGE_EXTENDER . [in] parametersAn EmberNetworkParameters value that specifies the network parameters of the network with which the node should associate.
- Returns
-
An
EmberStatusvalue that indicates either:- that the association process began successfully or
- the reason for failure.
◆ emberJoinNetworkExtended()
| EmberStatus emberJoinNetworkExtended | ( | EmberNodeType |
nodeType,
|
| EmberNodeId |
nodeId,
|
||
| EmberNetworkParameters * |
parameters
|
||
| ) |
Cause the stack to associate with the network using the specified network parameters. It can take several seconds for the stack to associate with the local network. Do not send messages until a call to the emberStackStatusHandler() callback informs you that the stack is up. Notice that forming a network causes the node's security frame counter to be reset.
- Parameters
-
[in] nodeTypeSpecification of the role that this node will have in the network. This role can be EMBER_STAR_RANGE_EXTENDER , EMBER_STAR_END_DEVICE , EMBER_STAR_SLEEPY_END_DEVICE , EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE . If the node is frequency hopping, the role can not be EMBER_STAR_RANGE_EXTENDER . [in] nodeIdAn EmberNodeId value indicating the short ID the node intends to use for addressing purposes. If this value is EMBER_NULL_NODE_ID , the network coordinator will allocate a new short address. Addresses should be allocated by the coordinator unless there is a specific need to join a network with a specific ID. If a specific ID is used, uniqueness should be guaranteed across the entire network by the application, via some out of band means. Notice that nodes of EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE require this parameter to be set to EMBER_NULL_NODE_ID . [in] parametersAn EmberNetworkParameters value that specifies the network parameters of the network with which the node should associate.
- Returns
-
An
EmberStatusvalue that indicates either:- that the association process began successfully or
- the reason for failure.
◆ emberMacAddShortToLongAddressMapping()
| EmberStatus emberMacAddShortToLongAddressMapping | ( | EmberNodeId |
shortId,
|
| EmberEUI64 |
longId
|
||
| ) |
An API to populate the short-to-long address mapping table at the MAC layer. The table is meaningful only when running as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE . The standard 802.15.4 encryption and authentication process requires the security nonce to be populated with the source node long ID. A receiver must do the same to decrypt a secured incoming message. This short-to-long mapping table is used to decrypt a secured incoming packet from a node using short source addressing. If no entry is found in this table, the incoming message will be dropped. This table is also used to encrypt secured outgoing messages with short source addressing in case the node is sending out a secured message with a short source address other than its own.
- Note
- Because the table is stored in RAM, the application should ensure it gets correctly re-populated upon reboot.
- Adding a new entry will cause the removal of existing entries matching the passed short ID or long ID.
- Parameters
-
[in] shortIdThe short address of the [short, long] entry to be added to the table. [in] longIdThe long address of the [short, long] entry to be added to the table.
- Returns
-
an
EmberStatusvalue of:- EMBER_SUCCESS if the mapping was successfully added to the table.
- EMBER_INVALID_CALL if the node is not running as EMBER_MAC_MODE_DEVICE or as EMBER_MAC_MODE_SLEEPY_DEVICE .
- EMBER_TABLE_FULL if the table is currently full.
- EMBER_NO_BUFFERS if the heap does not currently have enough space for the new entry. The size of the table is controlled by the EMBER_SECURITY_SHORT_TO_LONG_MAPPING_TABLE_SIZE .
◆ emberMacClearShortToLongAddressMappings()
| EmberStatus emberMacClearShortToLongAddressMappings | ( | void |
|
) |
An API to clear the short-to-long address mapping table at the MAC layer.
- Returns
-
an
EmberStatusvalue of EMBER_SUCCESS if table was , or anotherEmberStatusvalue indicating the reason of failure.
◆ emberMacFormNetwork()
| EmberStatus emberMacFormNetwork | ( | EmberNetworkParameters * |
parameters
|
) |
Form a new network as an EMBER_MAC_MODE_DEVICE by becoming the coordinator. This API should be used to form a compliant 802.15.4 PAN and to inter-operate with other 802.15.4 devices. Notice that forming a network causes the node's security frame counter to be reset.
- Parameters
-
[in] parametersAn EmberNetworkParameters value that specifies the network parameters of the network to be formed.
- Returns
-
An
EmberStatusvalue that indicates either the successful formation of the new network or the reason that the network formation failed.
◆ emberMacSetPanCoordinator()
| EmberStatus emberMacSetPanCoordinator | ( | bool |
isCoordinator
|
) |
Configure a EMBER_MAC_MODE_DEVICE node to be a PAN coordinator. Note, this only applies to nodes that have been commissioned as EMBER_MAC_MODE_DEVICE .
- Parameters
-
[in] isCoordinatorIf set to true, the node will identify itself as the PAN coordinator.
- Returns
-
An
EmberStatusvalue of EMBER_SUCCESS if the coordinator flag was successfully set, or anotherEmberStatusvalue indicating the reason of failure.
◆ emberNetworkInit()
| EmberStatus emberNetworkInit | ( | void |
|
) |
Resume the network operation after a reboot.
This API must be called on boot prior to ANY network operations. It initializes the networking system and attempts to resume the previous network identity and configuration. If the node was not previously joined, this routine should still be called.
If the node was previously joined to a network, it will retain its original type (e.g., coordinator, router, end device, and so on.)
EMBER_NOT_JOINED is returned if the node is not part of a network.
- Returns
-
An
EmberStatusvalue that indicates one of the following:- successful initialization,
- EMBER_NOT_JOINED if the node is not part of a network, or
- the reason for failure.
◆ emberNetworkLeave()
| EmberStatus emberNetworkLeave | ( | void |
|
) |
Allow a star topology node that previously joined a network to leave the network. The node will notify the parent node and eventually leave the network. The application is notified that the leave procedure completed via the emberStackStatusHandler() handler.
- Returns
-
An
EmberStatusvalue of EMBER_SUCCESS if the node successfully initiated the network leave procedure, or anotherEmberStatusvalue indicating the reason of failure.
◆ emberPermitJoining()
| EmberStatus emberPermitJoining | ( | uint8_t |
duration
|
) |
Tell the stack to allow other nodes to join the network with this node as their parent. Joining is initially disabled by default. This function may only be called after the node is part of a network and the stack is up.
- Parameters
-
[in] durationA value of 0x00 disables joining. A value of 0xFF enables joining indefinitely. Any other value enables joining for that number of seconds.
- Returns
-
an
EmberStatusvalue of EMBER_SUCCESS if the permit joining was successfully set, otherwise anEmberStatusvalue indicating the reason of failure.
◆ emberResetNetworkState()
| void emberResetNetworkState | ( | void |
|
) |
Forget the current network and reverts to a network status of EMBER_NO_NETWORK .
◆ emberSetActiveScanDuration()
| EmberStatus emberSetActiveScanDuration | ( | uint16_t |
durationMs
|
) |
Set the time in milliseconds the node will spend listening for incoming beacons during an active scan. The dafault value is set based on the symbol time of the current PHY configuration according to the 802.15.4 specs.
- Parameters
-
[in] durationMsThe active scan duration in milliseconds. A value of 0xFFFF restores the default value.
- Returns
-
an
EmberStatusvalue of EMBER_SUCCESS if the active scan duration was successfully set, otherwise anEmberStatusvalue indicating the reason of failure.
◆ emberSetApplicationBeaconPayload()
| EmberStatus emberSetApplicationBeaconPayload | ( | uint8_t |
payloadLength,
|
| uint8_t * |
payload
|
||
| ) |
Allows the application to set the application portion of the beacon payload. It's by default set to the empty string.
- Parameters
-
[in] payloadLengthThe length in bytes of the application beacon payload to be set. This value can not exceed EMBER_MAC_MAX_APP_BEACON_PAYLOAD_LENGTH . [out] payloadA pointer to the application beacon payload to be set.
- Returns
-
an
EmberStatusvalue of EMBER_SUCCESS if the application beacon payload was successfully set, otherwise anEmberStatusvalue indicating the reason of failure.
◆ emberSetAuxiliaryAddressFilteringEntry()
| EmberStatus emberSetAuxiliaryAddressFilteringEntry | ( | EmberNodeId |
nodeId,
|
| uint8_t |
entryIndex
|
||
| ) |
Set an entry in the auxiliary address filtering table at a given address. Nodes of EMBER_DIRECT_DEVICE device type can receive incoming messages destined to any of the node IDs in the auxiliary address filtering table (while also receiving messages destined to actual node ID). If the passed node ID is EMBER_NULL_NODE_ID , the entry is cleared.
- Parameters
-
[in] nodeIdAn EmberNodeId value to be added to the auxiliary address filtering table at the passed entry index. [in] entryIndexThe index of the auxiliary address filtering table entry to be set.
- Returns
-
An
EmberStatusvalue of EMBER_SUCCESS if auxiliary address filtering table entry was successfully set. AnEmberStatusvalue of EMBER_INVALID_CALL if the passed entry index is invalid.
◆ emberSetSelectiveJoinPayload()
| EmberStatus emberSetSelectiveJoinPayload | ( | uint8_t |
payloadLength,
|
| uint8_t * |
payload
|
||
| ) |
When invoked at a EMBER_STAR_COORDINATOR or a EMBER_STAR_RANGE_EXTENDER , it causes the stack to only accept subsequent joining nodes with matching joining payload. When invoked at a node that has not yet joined a network, it sets the joining payload that will be included in the joining process. Notice, the join payload is included in a non-standard 802.15.4 command, therefore this feature is not available for nodes operating as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE .
- Parameters
-
[in] payloadLengthThe length in bytes of the passed joining payload. This can not exceed EMBER_MAX_SELECTIVE_JOIN_PAYLOAD_LENGTH . [in] payloadA pointer to the payload to be set.
- Returns
-
An
EmberStatusvalue that indicates either:- that the node successfully set the join payload.
- the reason for failure.
◆ emberStartActiveScan()
| EmberStatus emberStartActiveScan | ( | uint16_t |
channel
|
) |
Start an active scan. EMBER_SUCCESS signals that the scan successfully started. Upon receiving a beacon, the emberIncomingBeaconHandler() stack handler is called. At the end of the scanning procedure, the emberActiveScanCompleteHandler() stack handler is called. Note that, while a scan can be initiated when the node is currently joined to a network, the node will generally be unable to communicate with its PAN during the scan period. In particular, time-sensitive network operations might be affected because a scan operation will prevent any network operation for the duration of the scan.
Possible error responses and their meanings:
- EMBER_INVALID_CALL , the node is currently frequency hopping.
- EMBER_MAC_SCANNING , indicates an ongoing scan.
- EMBER_PHY_INVALID_CHANNEL , the specified channel is not a valid channel on the current platform.
- Parameters
-
[in] channelThe channel to scan.
◆ emberStartEnergyScan()
| EmberStatus emberStartEnergyScan | ( | uint16_t |
channel,
|
| uint8_t |
samples
|
||
| ) |
Starts an energy scan. EMBER_SUCCESS signals that the scan successfully started. At the end of the scanning procedure the emberEnergyScanCompleteHandler() stack handler is called. Note that, while a scan can be initiated when the node is currently joined to a network, the node is generally unable to communicate with its PAN during the scan period. In particular, time-sensitive network operations might be affected because a scan operation will prevent any network operation for the duration of the scan.
Possible error responses and their meanings:
- EMBER_INVALID_CALL , the samples parameter is invalid or the node is currently frequency hopping.
- EMBER_MAC_SCANNING , indicates an ongoing scan.
- EMBER_PHY_INVALID_CHANNEL , the specified channel is not a valid channel on the current platform.
- EMBER_NO_BUFFERS , the stack doesn't have enough memory at the moment to perform the requested scan.
- Parameters
-
[in] channelThe channel to scan. [in] samplesThe number of energy samples to be produced. Each sample is performed averaging the detected energy over X symbols time, whereas X depends on the selected PHY configuration and set by default to 8. The symbol time duration also depends on the selected PHY configuration.
◆ emberTick()
| void emberTick | ( | void |
|
) |
A periodic tick routine that should be called in the main loop in the application.