Public Attributes#

void(*

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.

Routing slave to recieve route.

uint8_t

Destination of route (if 0 destination will be self). Destination can be a SUC.

uint8_t

Route to be assigned as priority route - set to zeroes to NOT supply a priority route (recommended)

uint8_t

Public Attribute Documentation#

Handle#

void(* SAssignReturnRoute::Handle) (void)

Definition at line 1395 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

ReturnRouteReceiverNodeId#

node_id_t SAssignReturnRoute::ReturnRouteReceiverNodeId

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.


Definition at line 1399 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

RouteDestinationNodeId#

node_id_t SAssignReturnRoute::RouteDestinationNodeId

Routing slave to recieve route.


Definition at line 1400 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

aPriorityRouteRepeaters#

uint8_t SAssignReturnRoute::aPriorityRouteRepeaters[4]

Destination of route (if 0 destination will be self). Destination can be a SUC.


Definition at line 1401 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

PriorityRouteSpeed#

uint8_t SAssignReturnRoute::PriorityRouteSpeed

Route to be assigned as priority route - set to zeroes to NOT supply a priority route (recommended)


Definition at line 1402 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

isSucRoute#

uint8_t SAssignReturnRoute::isSucRoute

Definition at line 1403 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h