Public Attributes#
void(*
bool
Placeholder for callback function.
uint8_t
False if frame rejected by protocol, can be due to content/configuration or due to timing (e.g. inclusion request when not in learn mode)
Public Attribute Documentation#
Handle#
void(* SZWaveTransmitStatus::Handle) (void)
Definition at line
1775
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
bIsTxFrameLegal#
bool SZWaveTransmitStatus::bIsTxFrameLegal
Placeholder for callback function.
Definition at line
1776
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
TxStatus#
uint8_t SZWaveTransmitStatus::TxStatus
False if frame rejected by protocol, can be due to content/configuration or due to timing (e.g. inclusion request when not in learn mode)
Definition at line
1777
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
ExtendedTxStatus#
TX_STATUS_TYPE SZWaveTransmitStatus::ExtendedTxStatus
Definition at line
1778
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h