Network Info.
Public Attribute Documentation#
eInclusionState#
EInclusionState_t SNetworkInfo::eInclusionState
Definition at line
1547
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SucNodeId#
node_id_t SNetworkInfo::SucNodeId
Definition at line
1548
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SecurityKeys#
uint8_t SNetworkInfo::SecurityKeys
Definition at line
1549
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
NodeId#
node_id_t SNetworkInfo::NodeId
Definition at line
1550
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
HomeId#
uint32_t SNetworkInfo::HomeId
Definition at line
1551
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
MaxPayloadSize#
uint16_t SNetworkInfo::MaxPayloadSize
Definition at line
1552
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h