Public Attribute Documentation#
Handle#
void(* SSendSlaveNodeInformation::Handle) (void)
Definition at line
1446
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
sourceId#
node_id_t SSendSlaveNodeInformation::sourceId
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
Definition at line
1449
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
destinationId#
node_id_t SSendSlaveNodeInformation::destinationId
Definition at line
1450
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
txOptions#
uint8_t SSendSlaveNodeInformation::txOptions
Definition at line
1451
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h