Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

nodeID#

node_id_t SCommandSetPriorityRoute::nodeID

Definition at line 1476 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

repeaters#

uint8_t SCommandSetPriorityRoute::repeaters[MAX_REPEATERS]

Definition at line 1477 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

routeSpeed#

uint8_t SCommandSetPriorityRoute::routeSpeed

Definition at line 1478 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

clearGolden#

uint8_t SCommandSetPriorityRoute::clearGolden

Definition at line 1479 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h