Public Attributes#

void(*
uint8_t

Public Attribute Documentation#

Handle#

void(* STest::Handle) (uint8_t, TX_STATUS_TYPE *)

Definition at line 1679 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

DestNodeId#

node_id_t STest::DestNodeId

Definition at line 1681 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

PowerLevel#

uint8_t STest::PowerLevel

Definition at line 1682 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h