Public Attributes#
int8_t
Db (negative) or EListenBeforeTalkThreshold_t.
Db (negative) or EtxPowerLevel_t.
Db (negative) or EtxPowerLevel_t.
int16_t
Maximum transmission power for Z-Wave LR.
RF Region setting.
uint8_t
Enable radio PTI.
Public Attribute Documentation#
iListenBeforeTalkThreshold#
int8_t SRadioConfig_t::iListenBeforeTalkThreshold
Db (negative) or EListenBeforeTalkThreshold_t.
Definition at line
1604
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
iTxPowerLevelMax#
zpal_tx_power_t SRadioConfig_t::iTxPowerLevelMax
Db (negative) or EtxPowerLevel_t.
Definition at line
1605
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
iTxPowerLevelAdjust#
zpal_tx_power_t SRadioConfig_t::iTxPowerLevelAdjust
Db (negative) or EtxPowerLevel_t.
Definition at line
1606
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
iTxPowerLevelMaxLR#
int16_t SRadioConfig_t::iTxPowerLevelMaxLR
Maximum transmission power for Z-Wave LR.
Definition at line
1607
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
eRegion#
zpal_radio_region_t SRadioConfig_t::eRegion
RF Region setting.
Definition at line
1608
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
radio_debug_enable#
uint8_t SRadioConfig_t::radio_debug_enable
Enable radio PTI.
Definition at line
1609
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h