Controller API.
Public Attribute Documentation#
Handle#
void(* SSetSucNodeId::Handle) (void)
Definition at line
1362
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SucNodeId#
node_id_t SSetSucNodeId::SucNodeId
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
Definition at line
1365
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
bSucEnable#
bool SSetSucNodeId::bSucEnable
Definition at line
1366
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
bTxLowPower#
bool SSetSucNodeId::bTxLowPower
Definition at line
1367
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
Capabilities#
uint8_t SSetSucNodeId::Capabilities
Definition at line
1368
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h