Public Attributes#

void(*

Will be returned with transmit status Allows application to recognize frames.

uint8_t

Public Attribute Documentation#

Handle#

void(* STransmitFrameConfig::Handle) (uint8_t txStatus, TX_STATUS_TYPE *extendedTxStatus)

Will be returned with transmit status Allows application to recognize frames.


Definition at line 1647 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

TransmitOptions#

uint8_t STransmitFrameConfig::TransmitOptions

Definition at line 1648 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

iFrameLength#

uint8_t STransmitFrameConfig::iFrameLength

Definition at line 1649 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

aFrame#

uint8_t STransmitFrameConfig::aFrame[TX_BUFFER_SIZE]

Definition at line 1650 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h