Public Attributes#

void(*
bool

Placeholder for callback function.

uint8_t

False if frame rejected by protocol, can be due to content/configuration or due to timing (e.g. inclusion request when not in learn mode)

Public Attribute Documentation#

Handle#

void(* SZWaveTransmitStatus::Handle) (void)

Definition at line 1775 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

bIsTxFrameLegal#

bool SZWaveTransmitStatus::bIsTxFrameLegal

Placeholder for callback function.


Definition at line 1776 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

TxStatus#

uint8_t SZWaveTransmitStatus::TxStatus

False if frame rejected by protocol, can be due to content/configuration or due to timing (e.g. inclusion request when not in learn mode)


Definition at line 1777 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

ExtendedTxStatus#

TX_STATUS_TYPE SZWaveTransmitStatus::ExtendedTxStatus

Definition at line 1778 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h