Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

bAnyRouteFound#

uint8_t SZWaveGetPriorityRouteStatus::bAnyRouteFound

Definition at line 1862 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

repeaters#

uint8_t SZWaveGetPriorityRouteStatus::repeaters[MAX_REPEATERS]

Definition at line 1863 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

routeSpeed#

uint8_t SZWaveGetPriorityRouteStatus::routeSpeed

Definition at line 1864 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h