Public Attribute Documentation#

Event#

e_application_security_event_t SReceiveSecurityEvent::Event

Definition at line 1996 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

iLength#

uint8_t SReceiveSecurityEvent::iLength

Definition at line 1997 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

aEventData#

uint8_t SReceiveSecurityEvent::aEventData[48]

Definition at line 1998 of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h