COMMON - Common Utilities
Description
General purpose utilities and cross-compiler support.
This SDK supports the following compilers/IDEs:
- Simplicity Studio
- IAR Embedded Workbench
- Keil µVision IDE
- Plain armgcc
Certain compiler features such as alignment is implemented differently in the tools. Therefore, macros such as SL_ALIGN are provided to enable compiler independent code.
- Note
- RAM code macros are implemented in a separate module RAMFUNC - RAM Function Support . Cross-compiler RAM code support needs extended documentation and it is therefore implemented as a separate module.
| Functions | |
| uint32_t | SL_CTZ (uint32_t value) | 
| Count trailing number of zeros. | |
| uint32_t | SL_RBIT (uint32_t value) | 
| Reverse the bits. | |
| uint32_t | SL_RBIT16 (uint32_t value) | 
| Reverse the bits. | |
| uint32_t | SL_Log2ToDiv (uint32_t log2) | 
| Convert logarithm of 2 to division factor. | |
| Macros | |
| #define | SL_CEILING (n, i) ((((n) + (i) - 1U) / (i)) * (i)) | 
| Round n up to closest interval of i. | |
| #define | SL_FLOOR (n, i) ((n / i) * i) | 
| Round n down to closest interval of i. | |
| #define | STRINGIZE (X) #X | 
| Stringify X. | |
| #define | SL_MIN (a, b) __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a < _b ? _a : _b; }) | 
| A macro for getting the minimum value. | |
| #define | SL_MAX (a, b) __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a > _b ? _a : _b; }) | 
| A macro for getting the maximum value. | |
| #define | SL_ATTRIBUTE_PACKED __attribute__ ((packed)) | 
| A GCC style macro for handling packed structures. | |
| #define | SL_PACK_START (x) | 
| A macro for handling packed structures. | |
| #define | SL_PACK_END () | 
| A macro for handling packed structures. | |
| #define | SL_ATTRIBUTE_ALIGN (X) __attribute__ ((aligned(X))) | 
| GCC style macro for aligning a variable. | |
| #define | SL_ALIGN (X) | 
| A macro for aligning a variable. | |
| #define | SL_WEAK __attribute__ ((weak)) | 
| A macro for defining a weak symbol. | |
| #define | SL_NORETURN __attribute__ ((noreturn)) | 
| A macro for handling non-returning functions. | |
| #define | SL_ATTRIBUTE_SECTION (X) __attribute__ ((section(X))) | 
| A macro for placing a variable in a section. | |
| #define | SL_FALLTHROUGH | 
| A macro for notifying the compiler of an intended switch case fallthrough. | |
| #define | SL_DEPRECATED_API_SDK_3_0 __attribute__ ((deprecated)) | 
| Macro for marking deprecated functions. | |
Function Documentation
◆ SL_CTZ()
| 
 | inline | 
Count trailing number of zeros.
Use CLZ instruction if available.
- Parameters
- 
         [in] valueData value to check for number of trailing zero bits. 
- Returns
- A number of trailing zeros in value.
◆ SL_RBIT()
| 
 | inline | 
Reverse the bits.
Use the RBIT instruction if available, else process.
- Parameters
- 
         [in] valueData value to reverse. 
- Returns
- A reversed value.
◆ SL_RBIT16()
| 
 | inline | 
Reverse the bits.
Use the RBIT instruction if available, else process.
- Parameters
- 
         [in] value16-bit data value to reverse. 
- Returns
- A 16-bit reversed value.
◆ SL_Log2ToDiv()
| 
 | inline | 
Convert logarithm of 2 to division factor.
- Parameters
- 
         [in] log2Logarithm of 2. 
- Returns
- Dividend.
Macro Definition Documentation
◆ SL_CEILING
| #define SL_CEILING | ( | 
            n,
            | |
| 
            i
            | |||
| ) | ((((n) + (i) - 1U) / (i)) * (i)) | 
Round n up to closest interval of i.
◆ SL_FLOOR
| #define SL_FLOOR | ( | 
            n,
            | |
| 
            i
            | |||
| ) | ((n / i) * i) | 
Round n down to closest interval of i.
◆ STRINGIZE
| #define STRINGIZE | ( | 
            X
            | ) | #X | 
Stringify X.
◆ SL_MIN
| #define SL_MIN | ( | 
            a,
            | |
| 
            b
            | |||
| ) | __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a < _b ? _a : _b; }) | 
A macro for getting the minimum value.
No sideeffects, a and b are evaluated one time only.
◆ SL_MAX
| #define SL_MAX | ( | 
            a,
            | |
| 
            b
            | |||
| ) | __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a > _b ? _a : _b; }) | 
A macro for getting the maximum value.
No sideeffects, a and b are evaluated one time only.
◆ SL_ATTRIBUTE_PACKED
| #define SL_ATTRIBUTE_PACKED __attribute__ ((packed)) | 
A GCC style macro for handling packed structures.
◆ SL_PACK_START
| #define SL_PACK_START | ( | 
            x
            | ) | 
A macro for handling packed structures.
        
        Use this macro before the structure definition.
        
        X denotes the maximum alignment of structure members. X is not supported with GCC. GCC always uses 1 byte maximum alignment.
       
◆ SL_PACK_END
| #define SL_PACK_END | ( | 
            | ) | 
A macro for handling packed structures.
        
        Use this macro after the structure definition.
        
        With GCC, add SL_ATTRIBUTE_PACKED after the closing curly braces of the structure definition.
       
◆ SL_ATTRIBUTE_ALIGN
| #define SL_ATTRIBUTE_ALIGN | ( | 
            X
            | ) | __attribute__ ((aligned(X))) | 
GCC style macro for aligning a variable.
◆ SL_ALIGN
| #define SL_ALIGN | ( | 
            X
            | ) | 
A macro for aligning a variable.
        
        Use this macro before the variable definition.
        
        X denotes the storage alignment value in bytes.
        
        To be GCC-compatible, use
        
         SL_ATTRIBUTE_ALIGN(X)
        
        before the semicolon on normal variables. Use
        
         SL_ATTRIBUTE_ALIGN(X)
        
        before the opening curly brace on structure variables.
       
◆ SL_WEAK
| #define SL_WEAK __attribute__ ((weak)) | 
A macro for defining a weak symbol.
◆ SL_NORETURN
| #define SL_NORETURN __attribute__ ((noreturn)) | 
A macro for handling non-returning functions.
◆ SL_ATTRIBUTE_SECTION
| #define SL_ATTRIBUTE_SECTION | ( | 
            X
            | ) | __attribute__ ((section(X))) | 
A macro for placing a variable in a section.
        
        Use this macro after the variable definition, before the equal sign or a semicolon.
        
        X denotes the section to place the variable in.
       
◆ SL_FALLTHROUGH
| #define SL_FALLTHROUGH | 
A macro for notifying the compiler of an intended switch case fallthrough.
◆ SL_DEPRECATED_API_SDK_3_0
| #define SL_DEPRECATED_API_SDK_3_0 __attribute__ ((deprecated)) | 
Macro for marking deprecated functions.
SL_DEPRECATED_API_SDK_<RELEASE> is used to mark functions that are deprecated and should not be used from a given version of the SDK. The accompanying SL_SUPPRESS_DEPRECATION_WARNINGS_SDK_<RELEASE> define can be set to suppress warnings generated when using deprecated APIs.