BURTC_Init_TypeDef Struct Reference

BURTC initialization structure for Series 2 devices.

#include <em_burtc.h>

Data Fields

bool start
 Start BURTC after initialization.
 
bool debugRun
 If true, counter will keep running under debug halt.
 
uint32_t clkDiv
 Clock divider.
 
bool compare0Top
 Set if Compare Value 0 is also top value (counter restart)
 
bool em4comp
 Enable EM4 wakeup on compare match.
 
bool em4overflow
 Enable EM4 wakeup on counter overflow.
 

BURTC initialization structure for Series 2 devices.

Field Documentation

◆ start

bool BURTC_Init_TypeDef::start

Start BURTC after initialization.

◆ debugRun

bool BURTC_Init_TypeDef::debugRun

If true, counter will keep running under debug halt.

◆ clkDiv

uint32_t BURTC_Init_TypeDef::clkDiv

Clock divider.

Supported range is 1-32768

◆ compare0Top

bool BURTC_Init_TypeDef::compare0Top

Set if Compare Value 0 is also top value (counter restart)

◆ em4comp

bool BURTC_Init_TypeDef::em4comp

Enable EM4 wakeup on compare match.

◆ em4overflow

bool BURTC_Init_TypeDef::em4overflow

Enable EM4 wakeup on counter overflow.