IADC_ScanTableEntry_t Struct Reference
IADC scan table entry structure.
      
       #include <em_iadc.h>
      
     
| Data Fields | |
| IADC_NegInput_t | negInput | 
| Port/pin input for the negative side of the ADC. | |
| IADC_PosInput_t | posInput | 
| Port/pin input for the positive side of the ADC. | |
| uint8_t | configId | 
| Configuration id. | |
| bool | compare | 
| Perform digital window comparison on the result from this entry. | |
| bool | includeInScan | 
| Include this scan table entry in scan operation. | |
IADC scan table entry structure.
Field Documentation
◆ negInput
| IADC_NegInput_t IADC_ScanTableEntry_t::negInput | 
Port/pin input for the negative side of the ADC.
        
       
◆ posInput
| IADC_PosInput_t IADC_ScanTableEntry_t::posInput | 
Port/pin input for the positive side of the ADC.
        
       
◆ configId
| uint8_t IADC_ScanTableEntry_t::configId | 
Configuration id.
◆ compare
| bool IADC_ScanTableEntry_t::compare | 
Perform digital window comparison on the result from this entry.
◆ includeInScan
| bool IADC_ScanTableEntry_t::includeInScan | 
Include this scan table entry in scan operation.